按数据手册设计了个充电电路给7.4V锂电池充电,在只接入12V电源时,BAT脚输出8.4V正常,但接入锂电池后,BQ2057W发烫严重,锂电池也在保护电路作用下变成无电压输出,BQ2057W有损坏的可能。请问这个电路有什么问题吗,求高手指导!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按数据手册设计了个充电电路给7.4V锂电池充电,在只接入12V电源时,BAT脚输出8.4V正常,但接入锂电池后,BQ2057W发烫严重,锂电池也在保护电路作用下变成无电压输出,BQ2057W有损坏的可能。请问这个电路有什么问题吗,求高手指导!
这么说不是应该是MOS管会发烫吗?还有我将0.2欧电阻换成1欧的电阻也还是一样的情况呀,按1欧的阻值算,mosfet的最大PD计算如下 (12-0.125-6)*0.125/1=0.734 w ,小于SI4435的PD值1w,这是怎么回事呢?谢谢!
将Q2拿掉验证是否发热得到明显改善。
这个STAT pin是一个三态输出,可以直接驱动外部小型LED,对于大多数指示LED而言驱动电流都够用了。谢谢!
还真是Q2的问题,拿掉后接入一个1K电阻和一个发光二极管BQ2057W就不会发烫那么厉害了,也能正常充电了,用万用表测量STAT脚电压为8.9V,应该就是这个电压直接加在Q2的b e端,电流过大引起的,谢谢Michael Yang的帮助!
不客气,如果还需要保持原定的CC充电电流,MOSFET的部分建议你更换一个能承受更大功率的.避免MOSFET在CC阶段过热,特别是在电池电压接近过放门限的CC充电阶段。谢谢!