This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【DIY】LM3447 可调光10w射灯



之前的帖子被删除有点郁闷,现在重新发帖。

我就按客户10.5W的一款COB射灯制作。

1,输入230VAC±10%,频率50~60Hz。

2,输入功率10.5W,考虑到80%的效率,输出功率8.4W。使用夏普1512灯珠

3,兼容前切和后切调光。

4,输入输出隔离。