反激设计算中,我查阅了一些书籍,说由稳态下变压器磁平衡,Vindcmin*Dmax=Vf*(1-Dmax),请问这个式子究竟适合DCM还是CCM,还是说两种模式都可以同样用来求Dmax?是不是到后面计算电流的时候,由能量守恒定律,CCM模式下:1/2*(Ip1+Ip2)*Dmax*Vindcmin=Pout/η,DCM模式下:1/2*Ip*Dmax*Vindcmin=Pout/η,才是CCM和DCM模式设计的区别???高手赐教~~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
反激设计算中,我查阅了一些书籍,说由稳态下变压器磁平衡,Vindcmin*Dmax=Vf*(1-Dmax),请问这个式子究竟适合DCM还是CCM,还是说两种模式都可以同样用来求Dmax?是不是到后面计算电流的时候,由能量守恒定律,CCM模式下:1/2*(Ip1+Ip2)*Dmax*Vindcmin=Pout/η,DCM模式下:1/2*Ip*Dmax*Vindcmin=Pout/η,才是CCM和DCM模式设计的区别???高手赐教~~~
这个不清楚30%负载临界模式怎么算出满载ccm初次级峰值的,请王工说清楚下谢谢哈~~
在最低输入电压下,如果负载30%,占空比最大,增加负载进入连续模式,那么进入连续模式后占空比可以认为基本不变,而且电流变化值也不变,根据输出功率可以得到输入平均电流,然后根据占空比,电流变化值不就可以计算峰值电流了吗?
我觉得重要的一点是,注意DCMB的状态的工作特性,这种状态下既符合DCM的工作特性,又符合Flyback的公式:Vout=Vin*D/N*(1-D).根据这个去设置你要的DCM和CCM的工作点