This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100是否可以在持续充、放电电流60A下精准计量电池组电量?

Other Parts Discussed in Thread: BQ34Z100

 

Sheldon Cai(TI公司的):

                   您好!请问

                   项目 1、BQ34Z100是否可以在持续充、放电电流60A下能精准计量电池组电量?检流电阻值可以设置在2mΩ以下吗?在软件要怎样改?电池组总容量:59.8Ah(以60Ah算吧),电池组串数:7S,最高电压:29.75V,锂电池。

                   项目2、BQ34Z100用在铁锂电池上吗?在充、放电电流30A下能精准计量电池组电量?检流电阻值可以设置在5mΩ以下吗?在软件需要怎样设置处理?8串铁锂电池,电池组总容量:36Ah,最高电压:29.2V。

谢谢!

 

  • 1.需要在校准时按比例缩小电流数值,比如采用5A电流去校准时填写校准值为2.5A,然后将相关容量等数值缩小1倍,这样子的话能够使电量电流能够支持到60A,2mOhm应该可以使用,但是需要注意的是采样电阻小了之后低电流时电流精度会下降也容易受到噪声影响

    2.铁锂上这个芯片是支持的,但是由于铁锂本身放电曲线比较平坦,电量计计量相对钴理困难

     

  •  

    Sheldon Cai:

                 1、我们客户是用LCD屏显示的,相关的容量等参数要缩小1倍,这样在显示容量时的容量值会不会也相应的小1倍呢?或者是LCD显示那边要怎样处理?

                    如果我用5m或者1m的也是按照你说的方法去校准吗?

               2、用在铁锂电芯的在参数设置与电量学习时需要注意哪方面呢?相关的参数设置是不是与锂电池的设置相同?

               我的PCB(7串锂电池与8串铁锂共用一款板)板刚刚已经回来了,所以需要你的协助。谢谢!

     

  •  

    更正错误:

           “如果我用5m或者1m的也是按照你说的方法去校准吗?”更正为:如果我用5mΩ或者1mΩ的也是按照你说的方法去校准吗?

            

  • 1.这个问题也不难解决,SOC是一样的直接显示即可,容量的话可以乘以相应系数再显示

    2.铁锂电池需要的静置时间更长,与电池相关的从参数可能不一样。