This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于充电IC BQ24297

Other Parts Discussed in Thread: BQ24160, BQ24297, BQ24196, BQ24296, BQ24192, BQ24195

你好,

        之前我们产品使用充电IC BQ24160, 有两路输入:

1,USB,最大电流限制为1.5A

2.DC 输入2.5A.

现在我们的设计一台平板,充电电流期望在3A以上。TI产品bq24297应该能符合我们的要求。

但发现该芯片只有USB输入。根据USB BC1.2 规定,PD只能从DCP or CDP draw 1.5A 电流。

即使对于DCP or CDP 输入电流限制为3A, Micro USB cable和连接器能承受这么大的电流吗?