我用的是lm2596-12 ,我问一下,lm2596-12 能输出-12v的电压吗
如果可以,我输入12v的电池电压,能不能输出-12v的电压?还是输入电压必须高于12V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问您的这个-12V电压是用来给运放供电么?输出电流要求多大呢?如果输出电流在200mA以内,可以考虑用TPS7A3001,这是一颗允许负电压输入的LDO,可以实现你所要求的负压输入,负压输出。
可以考虑用flyback输出正负12V后,再用DC/DC转成正负5V。如果正负5V的输出功率在3W以下,可以考虑用LM5017做flybuck输出正负5V。整体的效率可以达到80%以上
guofeng yin 说:你好,我们是在参加2014年四川省TI杯电子设计比赛,是在为整个系统做电源,功率要求不高,但是对效率有要求,使用LDO芯片效率会不会很低?要求从220v市电接出正负12v,正负5v电源,效率大概80%以上,网上几乎都是7812,7912,7805,7805的方法,我自己觉得不太满意所以想到了开关电源,前辈有没有效率更高的推荐方案?谢谢!
你好,是这样的,你12V直接转5V使用LDO肯定效率低了,效率41.7%,你可以先用12V转到6V,然后再用LDO,其实这样看你负载是什么,再看要不要用LDO。
guofeng yin 说:你好,我们是在参加2014年四川省TI杯电子设计比赛,是在为整个系统做电源,功率要求不高,但是对效率有要求,使用LDO芯片效率会不会很低?要求从220v市电接出正负12v,正负5v电源,效率大概80%以上,网上几乎都是7812,7912,7805,7805的方法,我自己觉得不太满意所以想到了开关电源,前辈有没有效率更高的推荐方案?谢谢!
你这个题目是让你输出正负12V和正负5V吗?直接一个flyback不就可以了,也可以用两级,但是对变换器效率要求就高些,你可以做两种方案。
建议你单级选UCC28910,两级的可以前级输出个15V,然后再来一级LM5017的flybuck就比较有特色了。
祝你好运。