BQ24103 用来充 3节,10F/节,2.7V/节, 的超级电容适合否?
需要控制 电流在 1A 内,充完 电压为8V,用这种锂电池充电管理芯片适合不?
或者是否有其它更适合的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
Q1和Q3这两个MOSFET在充电器的设计中经常会看到,其中Q1是用来防止超级电容反向放电,即防止倒灌电流;Q3是一个用来限制开机时涌浪电流的,因为充电器输出端和系统负载(具有power path功能时)都是有容性负载的,如果没有这个Q3,开机时会出现比较大的涌浪电流在开机时给这些容性负载充电,有了这个Q3,通过Q3端的C24,我们可以减慢g-s电压的建立,让这个开机的过程变得平滑,因为mosfet的跨导限制了允许流过的最大电流,所以就不会出现那么大的涌浪电流。
谢谢!