This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

串联使用TPS62160会导致系统不稳定吗

Other Parts Discussed in Thread: TPS62160

我使用TPS62160产生3.3V,然后用另外一个TPS62160从3.3V产生1.8V。 这样使用是否有可能两个芯片间出现类似谐振的效应,导致噪声的增加?

在串行使用DC/DC的时候,如果DC的开关频率都很接近的话,是不是就容易有不稳定的现象?

  •     Hi

           或许是你需要得到3.3V,所以采用了2级转换,但是就过去的经验对于多级转换中,并没有造成噪声叠加或者谐振的现象等严重noise的问题

           建议你在两级的输入都增加一个0.1uF的陶瓷电容,第二级输入或者可以再并联一个10uF电容。

           就现在的转换而言,请协助做如下测试以确认问题:

           1. 断开2级连接,看3.3V输出是否稳定,然后外部电源给3.3V到第二级,看1.8V输出是否稳定?

           2. 如果不能稳定,将查看一下你的layout,TPS62160的输入电容需要10uF(可以大于)的陶瓷电容,并且layout尽量要靠近芯片Vin脚,走线要宽,避免寄生电感造成震荡。而输出电容也尽量靠近输出的电感,电感要尽量靠近SW,SW脚在的pad要尽量宽一点并且很规则,可以参考datasheet,这个也是为了避免产生寄生电感。

           3. 如果外部电源给3.3V到第二级都稳定了,你需要确认第一路在此3.3V负载下是否能稳定工作?

  • 可能会有些共模的干扰,布板的时候多注意一下。

  • 为什么要这么做呢?两级降压的效率当然比一级降压低,请问你的输入电压是多少?可以从输入通过TPS62160产生1.8V