This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28019 闭环问题



给芯片7脚供应12V,4脚(VINS)提供大于1.5V电压,6脚(VSENSE)提供大于0.8V电压,输出最大占空比,98%。调节6脚电压到4.8~5.2V,调节4脚的电压。

问题: 当6脚是4.9V时,调节4脚电压在2~6V变化,占空比不变(即最大占空比)(如果理解为:28019电流环采用单周期控制,当空载时,没有电流,导致占空比

最大。那何时稳定?);4脚只是起到保护的作用,对于调节没有影响;

当6脚是5V或者多一点,占空比下降到0;这是什么原因?