This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucd9222看不到脉冲波形&下载问题

Other Parts Discussed in Thread: UCD9222

TI工程师你好:

      我正在调试ucd9222+ucd97242的电源,为c6678提供两路核电压。电路设计参考研华的开发板。 配置文件是自己用offline fusion生成的。

      在fusion gui中可以查看到ucd9222。由于担心电压不对,烧毁器件。所以将电感去掉了。。测量电感前端的波形,发现一直是低电平。在fusion中的Vin监 视值是1.5V左右。我测量了ucd9222的电源脚,是3.3V。

     请问: 1、这种方法调试是否可以。去掉电感后,如果正常的话,电感前端是不是应该有脉冲波形?

                  2、怎么看ucd9222是否下载成功了呢?

                  3、如果下载成功的话,Vin的监视值是1.5V,会有哪些可能的原因造成呢?