另外,BQ24061手册中,举例设置的电流为750mA,设置为这个电流值有什么考虑吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
规格书中的750mA只是一个举例,如果一定要说它有什么特别的考虑,那么这个电流相对1A充电电流来说保留了适当的俗量,如果客户选择的电流值在750mA或750mA以下 相对这款芯片而言芯片是工作在一个应用环境很轻松的情况下,不会触及芯片的极限的状态。
当然实际选择的CC电流首要考虑的还是基于电池的化学特性来决定的所用的CC电流比率。谢谢!
谢谢!
电池规格书中,最大充电电流为1.5A,那么对于BQ24061,把充电电流设置为1A,不用考虑裕量,没什么问题吧?
你看一下电池的规格书 看写的标称容量(满充容量)是多少,比如是1000mAH,那么一般都建议用0.5C的电流充,即0.5×1000mAH/H=500mA.或者你把规格书发上来我帮你看一下,谢谢!
CC电流设置为1A是没有问题的,注意芯片的散热设计,底部的thermal pad焊接好。如果你的输入电压比4.2V高很多,那么建议你一个开关模式的充电器,如果输入电压比较接近4.2V,那么可以用这种线性充电器,这主要是效率和散热方面的考虑,谢谢!