如题,UC3854没有加散热,电流采样电阻温度70~80度或更高,mos管耐压600V,反向二极管耐压450V,只给uc3854供电时,输出占空比很大
问mos管突然短路烧毁(保险丝一同烧毁)的可能原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,UC3854没有加散热,电流采样电阻温度70~80度或更高,mos管耐压600V,反向二极管耐压450V,只给uc3854供电时,输出占空比很大
问mos管突然短路烧毁(保险丝一同烧毁)的可能原因
datasheet上的demo采样电阻两端电压典型值为0.25*6=1.5V,我设计的为0.05*10=0.5V,会对芯片工作情况有影响吗?
还有我用的是两个贴片4W的电阻并联,设计功率10*10*0.05=5W<8W,应该满足,可是电阻在电流3、4A时发热脚很严重,70度以上
理论上规格是这样,但是你目前的应用情况是MOS占空比很大,接近短路,所以你可以测试一下实际电流的波形
SLoan Kong 说:datasheet上的demo采样电阻两端电压典型值为0.25*6=1.5V,我设计的为0.05*10=0.5V,会对芯片工作情况有影响吗?
还有我用的是两个贴片4W的电阻并联,设计功率10*10*0.05=5W<8W,应该满足,可是电阻在电流3、4A时发热脚很严重,70度以上
C50一直在用0.1uF电容,原理图上没有改,发热问题解决了,只是用功率分析仪测效率只到90%,目前无功功率加到1600W,可是理论上能达到99%,
问题除了你指出的4点外,还有其他因素影响芯片的矫正效率吗?
"对于100K开关频率下,电压通常环做10Hz左右,电流环做到几KHz"
这句话是什么意思?怎么设计可以控制电压电流环的频率?
下午实验时UC3854又失控一次,烧毁mos管和保险丝。