This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

12V电池供电,变换出+5V和-5V,+15V和-15V,求电源解决方案

12V电池供电,变换出+5V和-5V,+15V和-15V,求电源解决方案。要求噪声要尽可能低。

  • 有很多种方式来实现正负电压 ,具体的选择需要根据负载的特性来决定,常规情况下,用一个buck/boost电路和一个inverting电路(buck-boost,注这里不是指四管buck-boost模式智能切换电路),inverting电路用buck控制器改会有利于公司采购,减少器件型号。如LM22674 ,分别用它搭建输出5v的buck和-5v以及-15V的invering,用TPS61170搭建12v转15V的boost。以上转换器请确认一下输出电流是否满足你的规格,因为问题中没有给出负载大小。

    如果负电压的负载比较小,且调整比较小,那么对于+-5V的需求,可以用一个ccm的buck 再伴生一路DCM 的inverting(有输入线线性调整能力),这样一个dc-dc控制器实现两路输出,当然还有其他能量耦合的方法。对于负电压负载不大 着重强调精度高的场合下还可以用运放搭建一个反相器得到一个非常干净稳定的负电压。谢谢!