现在用BQ24061一路给电池充电,一路给负载供电,发现电池充满后,BQ24061停止工作了,因为可以从稳压源上看到供电电流只有7mA左右。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在用BQ24061一路给电池充电,一路给负载供电,发现电池充满后,BQ24061停止工作了,因为可以从稳压源上看到供电电流只有7mA左右。
谢谢!
也就是说充电完成后,充电IC并不停止工作,还会给后级负载供电?
你这个给后级负载供电的电路图是否能发上来?BQ24061本身没有带路径管理.谢谢!
就是在out端既接了电池,也给后级供电,后级负载的电流约为100mA左右!!
一般这样做不插拔的结构时会将max charge timer功能禁止,同时将充电截止也禁止;
如果一定要做可插拔的结构,那么就用外部分立器件搭建一个路径管理电路,请参考如下一个帖子,谢谢!
http://www.deyisupport.com/question_answer/analog/battery_management/f/35/p/24355/85881.aspx
谢谢!
我做了一个实验,用一个4.1V的电池进行充电,IC的保护时间为5个小时,大约充了3个小时后,电流就掉为7mA了。现在的问题是,充电时间没有超过保护时间,为什么充电IC就关断了?