调试TPS40200 ,输入30v,输出12v
现象:1.输入24v以上电压带载(轻微的也一样)开机,IC 不停重启,将输入电压30v往低调,到24v左右,ic进入正常工作
2.板子不接电子负载任意电压开机,正常工作,突然加载则IC进入进入重启
外围电路不复杂,怎么调都不能根本解决问题。我把SS端的电容去掉,电路可带载良好工作。另外有人说是电容太小(22uf),我并联四个电容还是不行
求解
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
调试TPS40200 ,输入30v,输出12v
现象:1.输入24v以上电压带载(轻微的也一样)开机,IC 不停重启,将输入电压30v往低调,到24v左右,ic进入正常工作
2.板子不接电子负载任意电压开机,正常工作,突然加载则IC进入进入重启
外围电路不复杂,怎么调都不能根本解决问题。我把SS端的电容去掉,电路可带载良好工作。另外有人说是电容太小(22uf),我并联四个电容还是不行
求解
Hi
输入电容100uF的耐压值是不够的,需要改成50V的。输入电容100uF需要layout到芯片VDD的大Pad上,2.2uF电容尽量Vdd脚。
高压启动不正常,而低压启动正常,对于buck电路而言,看起来电路是没有什么问题的,如上将输入电容修改后测试看看?
你好,我发现改动comp 频率反馈效果明显,但离我的要求有差距---我需要输出12v带载3A
SS 的电容电阻我都动过,实际效果有限,基本判定不是ss 设置问题。如下请了解
你好,我发现改动comp 频率反馈效果明显,但离我的要求有差距---我需要输出12v带载3A