Other Parts Discussed in Thread: LM3447
各位大侠,请问有没有原边控制的开关电源,用于LED驱动,输入85-265VAC,输出为,恒流500MA 10V,万请各位指教!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
mingyuan zhang 说:各位大侠,请问有没有原边控制的开关电源,用于LED驱动,输入85-265VAC,输出为,恒流500MA 10V,万请各位指教!
您需要的是全电压范围的驱动吗,请问是什么应用呢?
目前TI的LM3447可以做到全电压范围。不过您的输出5W/10V有点小哦。
所以输入电压是85Vac到265Vac?
有需要做成调光的吗?
mingyuan zhang 说:要求是出中国大陆这边了,我是想全电压的话,我其他客人也可以了,这次他们要求不要调光的,因为加了高调光价格会高,是要冲量了,各位看看有没有比较质优价廉的案子,推一下,谢谢各位了
全电压的话目前可以选择LM3447的方案,已经过了EMC测试,不过它是有调光功能的。
其他选择的话,您可以参考http://www.ti.com/ww/en/lighting/bulb/selectortool.shtml。这是一个LED驱动参考设计的选型工具,希望可以帮到您。