Other Parts Discussed in Thread: LM5118, LM3481, LMR14206, TPS54060, TPS54140, TPS54040, TPS54160
我现在想选一款 输入5-42V以内的 稳定5V输出 1A的DCDC或者500mA的ldo可有推荐? TI 的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
或者TPS54040 是3.5V 至 42V 输入、0.5A 降压转换器也是可以,TPS54060是其60V输入版本的,如果电流要到1A, 可以选择其1.5A版本的TPS54140和TPS54160.
选择比较多,可以用wenench软件筛选,然后在找你认为最适合的。