这个图我用的tps70933,可是怎么输入9v,输出只有不到1v,试了好几个芯片都这样,到底怎么回事啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
INPUT AND OUTPUT CAPACITOR
The TPS709xx are stable with output capacitors with an effective capacitance of 2.0 μF or greater for output
voltages below 1.5 V. For output voltages equal or greater than 1.5 V, the minimum effective capacitance for
stability is 1.5 μF. The maximum capacitance for stability is 47 μF. The equivalent series resistance (ESR) of the
output capacitor should be between 0 Ω and 0.2 Ω for stability.
The effective capacitance is the minimum capacitance value of a capacitor after taking into account variations
resulting from tolerances, temperature, and dc bias effects. X5R- and X7R-type ceramic capacitors are
recommended because these capacitors have minimal variation in value and ESR over temperature.
Although an input capacitor is not required for stability, it is good analog design practice to connect a 0.1-μF to
2.2-μF capacitor from IN to GND. This capacitor counteracts reactive input sources and improves transient
response, input ripple, and PSRR. An input capacitor is necessary if line transients greater than 10 V in
magnitude are anticipated.
不要电解电容,只要陶瓷电容
输入电容:4.7uF/25V
输出电容:4.7uF/10V或者4.7uF/16V
http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=slvu689a&fileType=pdf
这个是User guide,请参考电路和测试结果,没有问题啊