This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610的/ACDRV输出方波

Other Parts Discussed in Thread: BQ24610

在没有接电池的情况下,BQ24610的3脚/ACDRV 的管脚波形如下,导致输出的12V也是方波。

测量芯片的时候,

ISET1=0.3V

ISET2=0.3V

ACSET=0.54V

VREF=CE=3.3V

TS=1.64V

TCC接地。

VCC=12V