您好,我在做高温实验时遇到这样一个问题;温度箱温度105度时,观察到TPS70151的1.8V指示灯会灭大概0.5s后恢复(这时DSP 的CAN通讯中断),然后重复出现,测得此时TPS70151表面温度为140度左右。
请问这种现象是否与该芯片有关?急需解决,如需详细询问现象,请发邮件至kongshu@fcv-sh.com,非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我在做高温实验时遇到这样一个问题;温度箱温度105度时,观察到TPS70151的1.8V指示灯会灭大概0.5s后恢复(这时DSP 的CAN通讯中断),然后重复出现,测得此时TPS70151表面温度为140度左右。
请问这种现象是否与该芯片有关?急需解决,如需详细询问现象,请发邮件至kongshu@fcv-sh.com,非常感谢
Hi
芯片热热保护了,TPS70151的热保护温度是150℃,有个大约10℃的磁滞(datasheet没有说明这个规格),也就是说当芯片高出150℃芯片热shutdown, 之后芯片会降温,到达140℃后芯片恢复启动。
如果你的芯片使用环境必须要高达105℃,你需要采用更好的热设计,使得芯片结温在满负载(留一些裕量)都不会超过150℃.
或者你需要向办法降低芯片的环境温度,例如加风扇等。
Hi
如果是热关断应该是2路都关断的, 从芯片方框图看它是直接通过2路enable控制的。
(另外补充一下,热关断之后,芯片是在下降到130℃左右时才恢复启动的,见datasheet描述: If the temperature of the device exceeds+150°C (typ), thermal-protection circuitry shuts it down. Once the device has cooled below +130°C (typ),regulator operation resumes.)
芯片的结温推荐是低于125℃,如果要工作在105℃,那么芯片的温升只能有20℃,这样的话你需要尽量减小芯片的功耗(例如降低输入电压,但是这个一般已经由你的外部电源决定了,或者你可以采用分散的方式,例如在输入上增加一个二极管/大功率电阻等之类的方法,将部分热消耗在二极管上之类), 其次就是加强热设计,降低芯片热阻。