目前正在使用LM26420XMH/NOPB ,电路原理图如附件,需要同时供给出两路电压,其中Buck2输出3.3V,buck1输出1.2V,Vin输入范围是4.5—5.5,请问这样设计可行么?3.3V的输出是否会存在输出不稳定的状况?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前正在使用LM26420XMH/NOPB ,电路原理图如附件,需要同时供给出两路电压,其中Buck2输出3.3V,buck1输出1.2V,Vin输入范围是4.5—5.5,请问这样设计可行么?3.3V的输出是否会存在输出不稳定的状况?谢谢
Hi
可以的。
datasheet上有很多方案可以参考,你可以选择3.3V输出和1.2V输出的部分电路进行参考.(2路buck是独立的,主要改一下反馈电阻)
目前在依据上图的参考电路BUCK2 的输出电路是3.3V,其中电感是1.0uH,R1=31.6KF,R2=10KF,C1=22UF,EN直接通过串联1K电阻到输入,,输出的3.3V电压供给mAIX的DS1233A(复位芯片),希望用于监控电压,并提供复位信号(低有效),目前发现一个比较奇怪的现象:1:到输入给LM26420XMH/NOPB的电压低于5.0或者5.1V的时候,发现此时用示波器测量DS1233A的复位输出,会看见该信号周期性的拉低然后又变高;2、将输入调高到5.1V以上的时候检测时,该复位信号会一直为高并不会出现拉低的现象(除开初始上电的复位一下);在以上的两种情况下,都监测供给DS1233A的供电电压3.3V,均没有发现有任何异常的掉电或者升压的过程。
目前手头上有两块焊接有LM26420XMH/NOPB的板子,将两块板子的输出端的电感更换成1.5uH,发现其中一块在输入电压低于5V的时候复位信号不会周期拉低,另外一块还是存在该现象,求达人告知有没有什么解决办法