老师:
您好!我们需要一款单端数字驱动芯片用于驱动24~48个后级节点,要求开关速率能达到100MHz,驱动电流1~2A,信号压摆率2ns/3V,1.2ns/1V(20% to 80%),现在市面上很难找到满足该参数的芯片,因此打算通过选择一个开关速率能到100MHz的MOSFET作为后级驱动,不知道CSD17484F4能不能满足该需求,如果不行TI还有没有更快速率的MOS管?
如果有合适的高速P、N对管作为推挽输出就更好。
大致的实施框图请见下图。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
老师:
您好!我们需要一款单端数字驱动芯片用于驱动24~48个后级节点,要求开关速率能达到100MHz,驱动电流1~2A,信号压摆率2ns/3V,1.2ns/1V(20% to 80%),现在市面上很难找到满足该参数的芯片,因此打算通过选择一个开关速率能到100MHz的MOSFET作为后级驱动,不知道CSD17484F4能不能满足该需求,如果不行TI还有没有更快速率的MOS管?
如果有合适的高速P、N对管作为推挽输出就更好。
大致的实施框图请见下图。
谢谢!
Hi
TI这边的MOS 主要用于开关电源设计,而一般电源设计开关频率不会超过2MHz, 而你的应用严重超过2MHz.
所以我这这边没有合适的MOS可以推荐。
HI
直接在美国E2E发帖即可: https://e2e.ti.com/