是否可以实现LM5576芯片欠压检测(欠压为17V)。检测方式是查看是否有输出电压。
我尝试用对SD管脚端的检测电压,如果SD端电压是<1.225V,但是输出电压还是5V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是否可以实现LM5576芯片欠压检测(欠压为17V)。检测方式是查看是否有输出电压。
我尝试用对SD管脚端的检测电压,如果SD端电压是<1.225V,但是输出电压还是5V。
同时,也注意一下1.225V还有一定的容差
0.5V应该是进入shut down模式了,测试的时候可以同时关注一下VCC的电压
meng meng2 说:我测试了一下,如果SD引脚为0.5V左右的时候没有输出
具体的设计参考一下datasheet P16的公式14
- http://www.ti.com/lit/ds/snvs447i/snvs447i.pdf
Kevin Chen1 说:另外,你注意一下分压电阻的选择,以及芯片内部有5uA的电流源