This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34100在循环测试时充满容量、容量的百分比、电流等出现错误?

Other Parts Discussed in Thread: BQ34Z100

TI工程师、论坛社员:

            大家好!我用BQ34100在循环测试时发现充满容量、容量的百分比、电流等出现错误,

1、只要接上电,5个LED灯就会全部一起亮(我不明白规格书的第21页的LED指示设置的内容),不知道应该怎样设置。

2、充电时充了30分钟左右,电芯电压才3.5V,容量百分比就会到100%了,充电状态还在继续。

3、放电时也是几分钟后容量的百分比就会到0%了,放电状态还在继续。

4、充满容量也达不到设计时的23400mAh。

 5、在5A放电时会200多mA的误差(电流校准是以放电的-2000mA,当时校准后完成也有50多mA的误差)。

        请教应该怎样设置参数。

 

现在想这样分配5个LED灯,亮第一个灯0~20%;亮第二个灯21~40%;亮第三个灯41~60%;亮第四个灯61~80%;亮第五个灯81~100%。

检流电阻1mΩ(5个5mΩ并联),电芯总容量23.4Ah,电芯型号为ICR18650-26F,保护板持续放电电流20A(在调试中先用5A测试),7串的电池组。

 

BQ34Z100扫描截图在附件里,烦请各位指导该怎样设置参数。谢谢!

        另外:请问怎样把GG格式的文件添加到附件来?

 

 

BQ34Z100扫描截图.doc