我们的产品中批量使用了BQ24725,但前几天有一个设备的BQ24725模块出现了这样的问题,插入适配器(没有接电池)之后,ACOK的电平一直为低,同时BQ24725的CMSRC及ACDRD引脚都输出低电平(示波器观察的),但REGN输出是6V。根据手册上的描述我们又测量了一下三个点的电压:1.引脚ACDET的电压为2.75V,2.SRN引脚的电压为1.15V,3.VCC引脚的电压为13.5V,适配器供电电压为13.9V。根据测试结果我们分析芯片外围都是正常的,然后我们更换了一个BQ24725电路工作正常,插上适配器,ACOK的输出也为高了。我们想确认有问题的BQ24725是否已经损坏,是芯片的哪个模块损坏,同时应该采取什么措施避免呢?迫切希望得到回复!谢谢!