我有个设计,用到不少运放(tl072),为保持高动态范围,电路要求用双电源。输入电压为DC48/DC24,输出为+-12电源,电流分别为+12v,2A;-12,1A。
其实目的是单电源来转正负电源,希望用ic来做,但电路中不需要变压器,电感只能用331那样的功率电感。
ti有这样的ic没,在官网上看到电荷泵可以,但电流太小啊,最大60ma。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LMZ模块,集成电感,外部采用24V供电。
+12V输出,用LMZ14202;
-12V输出,用LMZ34002.
你到TI官网用webench电源设计工具,就可以找到自己需要的方案: