非常感谢您的方案
方案1,可行性比较高,主要一个问题就是转换效率太低,而且两级配合,两个开关芯片开关频率不同,彼此之间的开关噪声影响应该很大
方案2,多个并联使用,如果两个芯片配合得不好,可能会输出不一致,影响蓄电池寿命
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM25118是控制器,电流限制只在于开关驱动能力,所以需要添加独立驱动。
LM25118的驱动是CMOS类型的,还是选择驱动芯片好。
LM25118最大驱动电流在2A左右,选Qg小的管子可能推得动。
抱歉我没有参考电路,看看别人是否能帮上忙。