我的电路板上供电脑电源的指标是10V~30V,使用的是TMSF28027的MCU芯片,其他的外设使用的电源都是3.3V,电路板正常运行时电流在150mA左右,我用了两级LDO做电源7805+lp2980-3.3,但是压差太大有点发热,请问有什么更好的解决方法吗?用DCDC给MCU供电稳定吗?求推荐方案。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
qiang wang6 说:稳定的输出电流150mA测过,峰值不会超过200ma
用DCDC的话纹波会不会影响mcu稳定性?
DCDC的输出电压都有一定范围的,比如+/-5%,同时单片机的输入电压也有一定范围。
如果你是在担心可以考虑一级DCDC,加一级LDO实现。
参考你的输入电压和输出电流范围,可以考虑使用TPS54140。