使用TPS54233,输入电压12V转3.3V时板子电源正常,但是如果输入电压抬高到17V电源就开始出现问题了,请问有遇到过吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS54233,输入电压12V转3.3V时板子电源正常,但是如果输入电压抬高到17V电源就开始出现问题了,请问有遇到过吗?
问题已经解决了,是缓启动电容用大了,导致芯片工作异常,改小电容就好了,您说的8--18V,如果输入是25V或者28V,只是需要改下参数也可以正常工作的吧,芯片支持到28V的。
guangyi yuan 说:问题已经解决了,是缓启动电容用大了,导致芯片工作异常,改小电容就好了,您说的8--18V,如果输入是25V或者28V,只是需要改下参数也可以正常工作的吧,芯片支持到28V的。
帮Max回复一下,输入电压范围变化了,需要从新设计相关参数,比如电感输出电容等。