Other Parts Discussed in Thread: BQ24192, BQ24195, TPS2553
Ti的工程师你们好:
我想用BQ24195做一个移动电源,希望在外接+5V到VBUS时,能向电池充电,在接设备时,VBUS能向外供电,不知可否实现?数据手册中对于PMID到VBUS的FET没有说明,不知这个FET是怎么开启。或者能推荐另外的能实现此功能的芯片。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,我的意思就是在VBUS不在时,能有一路5V 从VBUS给外部供电
Q1这个开关是防倒灌MOSFET ,如果Vbus线没有输入源,那么这个MOSFET 不会导通。
这个器件用来给外部充电时,我们建议在PMID端加一个可选的USB开关TPS2511,因为当充电器没有插入时 只有PMID的输出电压才会boost到5V来模拟USB母线电压来给外部电池充电。谢谢!
你好,没看明白。 我不是楼主,不过我也有和楼主同样的问题
我想知道VBUS没有电时,也就是没有插入充电器的时候PMID是否有5V输出?
这个关乎我的系统是否能用,因为我的系统需要不充电的时候能输出5V工作
PMID的作用就是在没有Vbus的时候输出5V的,有Vbus电压时,Vbus电压直接传到PMID 从而使得PMID的负载一直都有5V电压,这是这个系统需要达到的设计功能。谢谢!
意思就是说BQ24195不能实现VBUS输出5V,5V是在PMID上。那我看到BQ24192有个USB OTG功能,这个芯片是不是能输出5V在VBUS上?
意思就是说BQ24195不能实现VBUS输出5V,5V是在PMID上。那我看到BQ24192有个USB OTG功能,这个芯片是不是能输出5V在VBUS上?
BQ24192可以在VBUS上产生5V输出电压,对于POWER BANK应用,如果共用一个输入输出口,可以考虑使用BQ24192,如果输入输出口是独立分开,可使用BQ24195。都需要在VBUS或者PMID输出端加限流开关以保证输出恒流,可以考虑TPS2553。