2节1.5V碱性电池供电,经过TPS61097-3.3升压后给MCU和CC2500供电,CC2500和MCU整体消耗电流25MA。带上负载升压不起来;请高手看看TPS61097
电感是用国产的,C1,C3 胆电容。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当VIN<2.5时,整机测试电流40mA. 而且测试升压后Vout=2.0V
1,请将10uF输出电容换为陶瓷电容,并靠近Vout脚焊接
2,检查你的电感是否有问题
我之前帮客户debug TPS61093,当时空载有电压输出,电压略低,带载输出电压迅速跌落,仔细检查发现电感焊接短接了
这个芯片很简单,仔细排查一下就没问题了
芯片整体效率在80%以上,所以不太可能自身消耗那么多。
请问工作时电感烫吗?(尽量用温度计测,手摸当心烫伤)
刚才看错了,以为40mA是换算过的。
输入3.3×25=82.5,输出2×40=80,输入输出接近,没什么问题。