This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问lm3481在输出只有几十UA时候芯片的的功耗是多少
芯片工作电流大约4mA。不过这颗没有对轻载作优化,所以轻载效率很低。
Yongjie Ma1 说: 请问lm3481在输出只有几十UA时候芯片的的功耗是多少
Datasheet里有一行表明,当设置的开关频率为40kHz时,工作电流3.7mA. 即使输出电流很低,应该也是在这个数量级。
ISUPPLY Supply Current (switching) See (4) 3.7 5.0 mA
有没有推荐的芯片,输入3~24V,输出4V左右,轻载时不到1MA
为什么要低到3V呢?非同步可以考虑一下TPS54331