Other Parts Discussed in Thread: BQ24195, BQ24295
画好电路图了,发现好像bq24195必须满足4个条件才能 升压?那我的电池系统岂不是一直需要有一个cpu工作去维护了充电芯片了?
这样是不是耗电呀?有好的方法吗?
我的系统是一个类似手机的系统,平时电池经过升压给一个5v系统供电,我本来想找个通过bq24195的pmid提供呢,发现是不是有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
195是需要主控IC的,建议可以看一下bq24295这个芯片。BQ24295 支持Host-free boost mode enable
看了下BQ24295,感觉可以用,正在改图中,英文资料的 第6页的SYS的TYPE应该是P,不是I,请修改
另外咨询下这里面多了一个QON管脚,说是控制处于shipping mode的,不懂这个是干嘛的,指教一下,谢谢
还有一个问题,为什么BQ24295里的应用图和195的有点区别,在VBUS前,295少了Q1和Q2,这是为何?为啥不需要?谢谢
1。Shipping mode是用来关断charger内部连接电池的MOS,主要是用在长时间存储时减小主板上漏电导致电池电量下降
2.这个应该是用于power bank防止升压时OTG电压倒灌到输入端