This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq2000输入电压范围

Other Parts Discussed in Thread: BQ2000

请问一下BQ2000能否应用于输入电压为5v的场合?按照数据手册上给出的那个应用电路要求输入电压为9-16V.

  • 可以的,输入5 V就可以通过一个RC滤波器后直接给芯片的VCC了,高于5V时采用稳压管得到的5V。谢谢!

  • 因为这个充电器本质是一个buck电路,所以不同的应用条件下 外部器件也不一样,根据保证进入CCM稳态的条件计算外部器件即可。在占空比比较极端的情况下,注意保证MOSFET能够正常的开关。谢谢!

  • MICHAEL YANG 你好!向你请教关于BQ2000的问题,我现在做一个充电器,充5节镍氢电池。采用11v电源供电,在样品的充电测试中发现。当改变输入电压时,充电电流会有变化。大概是电压增大1v ,充电电流增大约100mA,这一点我没明白。我理解的是采样电阻通过流过电流大小来调节占空比达到恒流的目的,充电电流应该不会随输入电压的小范围变化而变化。另保持输入电压不变,在对空电池充电时,电流会大一些,随着电池电压的升高,充电电流会慢慢下降,降额大概为70mA左右。我如何做能在输入电压不变的情况下,让充电电流恒定在+—20mA左右。

    BQ2000.pdf
  • BQ2000只能做BUCK使用吗?我想输入5V,给2节串联锂电池充电,这个能实现吗?