最近在做一个USB的项目,但USB的5V到设备终端时已经不足5V,可能为4.8V,也可能低于4.6V,但需要一个很好的±5V为AD和其它的模拟部分供电,电流约100mA,请问TPS65130在供电4.2~5V之间时,能否输出±5V?如果不可以,可否推荐一个能满足上述条件的电源管理芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用了这个TPS65133,当时疏忽了,现在发现个大问题,就是买不到货啊! 可否推荐个可替代的电源芯片? 此外,对于输入不是标准5V的情况(USB设备),能否推荐个可以用来给AD供电的转5V的电源芯片?