Other Parts Discussed in Thread: TPS5450, LM1085, TPS54622
我想问一下TPS5450的输入输出最小压差是多少?
输入电压9V,希望能输出能在8.5V,不知道能不能做得到。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
此外您提到:
YANBING WEN 说:我是脉冲输出,占空比是30%,最大输出电流大概是3A,
是说您的负载不重,所以控制器工作在DCM,同时pulse状态下?但同时要支持3A的情况?
YANBING WEN 说:是这个意思,不知道会不会好一点,另外我实际加载在负载上的电压是8V,8.5V已经考虑FET的压降了
9VIN-->8VOUT,使用TPS54622是可行的,但还是处于芯片的极限占空比情况。
YANBING WEN 说:我其实是需要一个带始能端的稳压块,电流要能输出3A。不知道有没有更合适的选择。压差要尽量小
那你就用TPS54622或者带使能的LDO。