采用LM2676设计的27v--5v电路,调试过程中连接LM2676 5v输出端口的所有芯片均被烧毁,连接到5v输出端的 220uF/10v的电容也被烧毁。调试第二块板子时在调试的过程中5v输出端连接的芯片也被烧毁。请问这是什么原因造成的?LM2676 5v输出端会不会在某种情况下过压,如果这种情况发生,原因是什么?注:并不是一上电后面的器件就烧了,刚上电时我用万用变测量输出为5v正常电压,在调试的过程中突然烧毁,两块板子都这样。希望大神能解决,感激不尽!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用LM2676设计的27v--5v电路,调试过程中连接LM2676 5v输出端口的所有芯片均被烧毁,连接到5v输出端的 220uF/10v的电容也被烧毁。调试第二块板子时在调试的过程中5v输出端连接的芯片也被烧毁。请问这是什么原因造成的?LM2676 5v输出端会不会在某种情况下过压,如果这种情况发生,原因是什么?注:并不是一上电后面的器件就烧了,刚上电时我用万用变测量输出为5v正常电压,在调试的过程中突然烧毁,两块板子都这样。希望大神能解决,感激不尽!
我把负载断开测试时LM2676输出大约为9v,但我使用的是5.0v的固定输出。我以为是芯片坏了,连换了两片,输出大概都接近9v。请问在什么情况下5.0v的固定输出会导致输出远大于5v。

上图是大概示意图,运行过程是:上电后程序控制继电器LS1使继电器连接到LM的5v输出端,然后不再断开,同时LM的输出VOUT1为后面芯片供电;继电器LS1的5v输出又连接到继电器LS2,LS2由程序控制接5v,还是地。以前测试时在上电之前测试输出LM2676输出端VOUT1的电压为5v,电压正常。但在调试过程中导致VOUT1所连芯片全部烧毁,且我两块电路板VOUT1所连的芯片均在调试的过程中全部烧毁(注:烧毁好像发生在继电器LS2反复接5v,和地的过程中)。今天我拆掉继电器LS2,即除了LS1后面的电容没有任何负载,测LM2676的电压为9v,换了两块芯片输出电压都接近9v,不知道问题出在哪?以前测试时LM2676输出电压时正常的。