你好,
设计BQ24070充电电路的时候,计算恒流充电电流和充电截止电流,需要用到VSET和KSET,VSET手册中说半充电时用1.25V,是单指指AC适配器模式的半充电模式还是包括了100mA的USB充电模式?
计算终止充电电流的时候,KSET选择一个值,计算终止电流,再看终止电流在不在IOBAT范围之内,我选择425,得到16mA,不在IOBAT范围之内,是不是KSET就应该选择450?究竟是怎么选择KSET的呢?
多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
设计BQ24070充电电路的时候,计算恒流充电电流和充电截止电流,需要用到VSET和KSET,VSET手册中说半充电时用1.25V,是单指指AC适配器模式的半充电模式还是包括了100mA的USB充电模式?
计算终止充电电流的时候,KSET选择一个值,计算终止电流,再看终止电流在不在IOBAT范围之内,我选择425,得到16mA,不在IOBAT范围之内,是不是KSET就应该选择450?究竟是怎么选择KSET的呢?
多谢!
VSET只针对FAST CHARGE CURRENT来说的,当mode high即AC mode时,ISET1 PIN来设定FAST CHARGE CURRENT,此时通过设定ISET2高或者低来决定使用VSET还是1/2VSET;如mode low即USB mode,那么ISET2来决定是100mA还是500mA充电电流。
KSET的选取直接参考你期望的充电电流是多少,比如期望电流为500mA,那么就选取KSET为425,如电流小于100mA就选取KSET为450,然后根据公式得到合适的Rset阻值。