This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq51013与bq500211加msp430组成的低功耗无线充电方案技术瓶颈

Other Parts Discussed in Thread: BQ500211

bq51013与bq500211加msp430组成的低功耗无线充电方案技术瓶颈,我们按照官方方案制作无线充电,遇到的问题为,(1)47.2k模式两个指示灯一直都不能亮,插电瞬间与充电过程都无反应(2)无源蜂鸣器在充电连接过程,在成功连接qi设备下,有5%的概率会响一声(3)用示波器观测发射器ping(vpp>20v),周期6.4s,一个周期内还存在小幅脉冲(vpp<3.8v),观测数字通信,发现基本可从包络读出0,1。现在遇到的问题是通信过程很难建立起来,即设备难以连接成功,就算成功连接后,也很容易再次丢失连接,且设备输出只有1.1v左右,远达不到电池充电的4.2v.我们电路选择参数基本按照ti方案走。有一点特别奇怪当我们把发射模块4*100nf谐振电容换成4*10nf反而能增加设备连接成功率。请问我们如何根据目前情况重新调整设计方案,?ti方案对于pcb布线要求是否非常严格?
   望给予技术支持!!
  • 你好!我购买了一套此方案做的无线充电器,发现BQ500211的Pin5 & Pin6短路了,维修时更换了一颗,但是现在遇到的情况是:上电开始时,蜂鸣器响一声,全桥MOS的驱动信号正常,但是4S后,上臂的两颗MOS Q1 & Q3 驱动信号一直为低电平,下臂的两颗MOS Q2 & Q5 驱动信号一直为高电平;Pin6的sleep信号一直为高电平;Pin46 Vsense持续为0.588V;Pin42 Isense逐渐上升到340mV,后降为0V。请帮忙解答为何会出现这种情况,我没有检查出来原因,请高手帮忙,谢谢!!