专家们:
附件是我的电路图,发现无法给电池充电。
可以用i2c正确读到寄存器,如下:
0: 30
1: 1b
2: 60
3: 11
4: b2
5: 9a
6: 3
7: 4b
8: 4
9: 80
10: 23
拔掉12V电源后,也无法自动升压。图中NC开头的器件代表不焊接。
拜托了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
确认vbus引脚有12V ,ce引脚已经拉低。
我发现我的D+/D_引脚悬空,导致了24195无法识别是什么电源。所以我在图中R6处焊接了330ohm ,R8焊接了1K电阻。
现在寄存器的值是:
0: 35
1: 1b
2: 60
3: 11
4: b2
5: 9a
6: 3
7: 4b
8: 94 95 84 跳变中
9: 80
10: 23
我测了我的电池电压是3.8V,reg8为94时代表处在precharge状态,但根据datasheet page15 中Battery Precharge to Fast Charge Threshold为3.0V,我电池电压大于3.0V,按道理应该不是precharge呀
您好,
对于BQ24195在上电后CE和OTG Pin脚都被拉低时,寄存器的默认状态就是充电使能,buck是不需要激活就工作的。除非出现了类似OVP的保护或进入了HIZ高阻模式,但从您给出的寄存器的值,设置都是默认值。REG09没有显示有任何fault;REG0[7]=0,没有进入HIZ模式,理论上buck一定是工作的。
您可以先去掉电池,排除电池的影响,在Vsys输出空载,D+/D-和CE脚OTG脚都正确时,Vbus上电后看看Vsys和Vbat的电压。
同时您也可以考虑换个BQ24195芯片,排除是否是芯片出问题了。
您的寄存器设置都是默认值,在您现在对D+/D-的设置下,输入限流默认为1.5A,同时您在ILIM pin脚上用了332欧姆的电阻的限流值约为1.59A,两者较小的起到限流作用;而BQ24195默认的在fast charging时的充电电流为2048mA,所以reg8会显示input DPM。您可以根据您的应用设置input current limit或fast charging时的charging current,还要注意watch dog的设置。
在8V时工作,说明芯片没有问题;12V不工作可能是有外部电路造成。