Dear all,
最近在看sluu904文件,对原理图中部分元件的功能不太理解,请教TI的工程师。
1.EVM 选择MultiCell 模式,假设外挂7S battery pack,J5连接器的5-6端子短接,7-8端子短接,Vbat+=28V,请问Q3,D7的作用?假如Q3导通,则REGIN引脚的电压等于Vbat+,远远大于IC datasheet规定的2.7~4.5V范围,是否会对IC造成损害?IC的供电是如何工作的?
2.是否可以提供IC的内部框图供参考呢?
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
最近在看sluu904文件,对原理图中部分元件的功能不太理解,请教TI的工程师。
1.EVM 选择MultiCell 模式,假设外挂7S battery pack,J5连接器的5-6端子短接,7-8端子短接,Vbat+=28V,请问Q3,D7的作用?假如Q3导通,则REGIN引脚的电压等于Vbat+,远远大于IC datasheet规定的2.7~4.5V范围,是否会对IC造成损害?IC的供电是如何工作的?
2.是否可以提供IC的内部框图供参考呢?
非常感谢!
Q3不会完全导通,把它当成有源电阻,S脚电压略低于G脚。
场效应管Q3处于饱和区,DS电压较大,但GS电压较低,贴近夹断区的位置。因为给芯片供电仅需较小电流,此时Q3起到降压限流作用。