Other Parts Discussed in Thread: BQ34Z100
Dear all,
SLUA450文件,2.4章节Update of Resistance中有这样一段话:
The wait time is 500 seconds by default, but later the update waiting time decreases if the maximal discharge duration(DF.Max Dsg Duration) is less than 500 seconds.
Waiting time can decrease to as short as 100 seconds.
我准备选用BQ34Z100,请教问题如下:
1.DF.Max Dsg Duration 看起来可以通过设置寄存器设置其值,请问具体是哪个寄存器呢,如何设置?
2.Waiting time 最短只能设置为100s,可以更短吗? 我们的应用是选用功率电池,容量1500mAh,以30A电流放电,大概能撑4min。
希望诸位有识之士帮忙解答,万分感谢!