Other Parts Discussed in Thread: TPS40057, LM2671, TPS5410
需要如下规格的直流变压IC
DC-DC 芯片,参数要求如下:
1、输入耐压23V以上,输出5V;
2、效率高,90%以上;
3、封装SOP/DIP,尽量小;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以考虑 TPS40057 http://www.ti.com/product/tps40057
主要规格如下:
输入耐压最大到40V;
输入电压 0.7V 到 35V;
选择好的管子,效率可以到90%