电池电芯为松下3100mAh,两串4并,所带附载为脉冲式,最大功率15W左右;
电池在带20%的电量时搁置12小时后,电量自动归为了零,目前问题还没有解决,请高手给予帮助。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电池电芯为松下3100mAh,两串4并,所带附载为脉冲式,最大功率15W左右;
电池在带20%的电量时搁置12小时后,电量自动归为了零,目前问题还没有解决,请高手给予帮助。
如果器件型号正确,建议你确认一下chem id是否选择合适,容量配置是否正确。谢谢!
如Luke所说,2串的方案建议使用带保护和均衡的电量计,成本要求比较高可以考虑使用2串的电量计BQ28400,bq27541+保护IC的成本与BQ28400差别不大。出现电量归零的现象可以从以下几个方面检查:
1.CHEM-ID是否是经过匹配的,一般不大建议直接使用默认或者根据电芯型号直接选择,应该通过一个CHEM-ID放电过程用MATHCAD进行匹配,另外注意ID号下载是通过bqEASY或bqCONFIG而不是直接在DATA FLASH里修改ID号码
2.检查是否存在offset的的问题,采用BQ27541EVM板下载相同的senc文件,进行校准然后连接看是否能够复现改现象
3.容量设置以及学习过程是否正确,可以检查一下搁置前的20%是否是真实数值还是0%才是真实的SOC
此主机通讯协议为I2C,所以选择了27541,之前使用的是V200版本,后来通过下载SENC文件升级到了G1版本就出现我这个问题 。
V200是否也是大容量并且连续放电?另外g1版本建议disable平滑功能。