input voltage range: 100V~800VDC, nominal voltage: 560VDC
output voltage/current: 24V/10A.
能否提供可行方案?
我的方案是双管正激,变压器驱动。但不确定,在如此宽的占空比变化范围内,驱动变压器能否可靠工作?尤其是在负载快速变化时,如从1A阶跃变化至10A.
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
双管正激的占空比不能超过50%,在你的这个应用很难设计占空比,因为输入太宽了。
变压器的风险是有可能复位不了,变压器饱和。
当然,双管正激没有直通的风险,也是有优点的。