This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ask for 100V~700V DC input, 24V,10A power supply solution

Other Parts Discussed in Thread: UCC28600, UCC28610

input voltage range: 100V~800VDC, nominal voltage: 560VDC

output voltage/current: 24V/10A.

能否提供可行方案?

我的方案是双管正激,变压器驱动。但不确定,在如此宽的占空比变化范围内,驱动变压器能否可靠工作?尤其是在负载快速变化时,如从1A阶跃变化至10A.

谢谢。