This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.检查一下REG08的数值是多少
2.检查一下电池电压是否过高达到恒压充电
3.是否有接其他负载
4.短路一下D+和D-
谢谢!
bq24296是使用PSEL PIN来获取是USB输入还是Adaptor输入[PSEL高表示USB输入,低表示Adaptor输入],不能悬空,你要改下板,也可以继续使用bq24295。
0到a寄存器内容:
5F
3B
20
11
B2
9C
93
4B
AC
80
C0
REG08的值为0xac,我在D+和D-上飞了一个电阻200欧姆的
发现充电电流为700mA,再上不去了
我在用adpator充电时,测得PMID管脚电压为4.8V这是为何?
这个片子是不是在adpator充电器时,PMID直接用VBUS的电,不需要电池的电吧?
另外请教手册里的REG08里的ICHG和REG0里的IINLIM有什么区别?不太理解
我现在设置REG02寄存器,如下所示,左侧是寄存器值,右侧是充电电流,单位mA
00 452
04 505
08 561
10 649
20 735
40 766
60 766
80 766
我的ILIM电阻已经改成130欧姆了,请问为何电流上不去了?