This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133充电时挑电芯吗?

Other Parts Discussed in Thread: BQ24133

BQ24133组成的充电电路,12V输入,电池组是两串8.4V,2600mAH的电池。
输入限流1.73A,充电电流设定为1.5A。电路用的是BQ24133 datasheet里面的典型电路。

目前发现,30台中,有两台,充电时,插入适配器,开始充电,大概过2~5分钟后,充电灯开始闪烁,12V的输入电流从1.02A下降到10mA左右,充电停止。大部分时间是充电过2~5分钟后开始异常,有时是一插上适配器就开始闪灯。

有查过BQ24133周边,都是OK的。更换由BQ24133组成的充电板,还是会闪烁异常。

目前发现,更换电池盒,即换一组电池,充电就OK。

电池盒里面只有3串2并的电池组,以及一个10K的温度检测电阻。刚开始怀疑是电池盒里面的10K温度检测电阻异常,更换一颗,还是无效果。

这个“异常”的电池盒用直流稳压电源8.4V 1.5A充电,也没异常,用负载机放电,也都是好的。

请教一下TI的工程师,电芯一般出什么问题时,会导致充电芯片停止充电?非常感谢~~~

  • LED闪烁说明有fault状态,fault状态包括charge suspend,input OV,batt OV,timer fault和电池不在位,你先排查下这些情形。你做交叉实验的时候有没验证过有问题的2快PCB换到其他电池包上是否一样不能充电?充电芯片通常只调整充电电压和电流以匹配电芯类型,不会在同一类型电芯应用中还有差别。

  • 换了其他几个电池包,都可以正常充电,就是用那两台有问题机器的电池包,充电会停止。

    但是这两个电池组,单独测试,1.5A充电正常,4A放电也正常。

  • 建议量测下2个不良电池包充电时的电压,TS PIN波形吧,怀疑可能和电池包的组装连线方式有一定关系,整体阻抗异常,可能触发到charger的保护,而是用独立电源不会保护。芯片的个体差异很小,也可以从你使用其他电池包,2个电路板还可以正常充电来判断电路板没有太大问题。