求助TI技术人员:
输入:直流9-60V 输出:10V5A的 恒流IC 用于LED车灯的方案有么?
有类似能做到60W的恒流方案也可以!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求助TI技术人员:
输入:直流9-60V 输出:10V5A的 恒流IC 用于LED车灯的方案有么?
有类似能做到60W的恒流方案也可以!
Eric Mo 说:求助TI技术人员:
输入:直流9-60V 输出:10V5A的 恒流IC 用于LED车灯的方案有么?
有类似能做到60W的恒流方案也可以!
您可以尝试用LM3429-Q1。
输入范围:4.5Vdc~75Vdc
输出电流(max):5A
输出范围:3V~72V
支持拓布:Boost ,Buck-Boost ,Sepic
调光方式:Analog ,PWM