Other Parts Discussed in Thread: TPS61221
我在使用TPS61221时,在输入电压0.7-3.3V时,输出能稳定到2.8V,不是3.3V,我使用的电感是10UH的,因为公司暂时没有4.7的,请问这个是不是原因所在啊
技术参数上也说电感要大于4.7UH的啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61221
我在使用TPS61221时,在输入电压0.7-3.3V时,输出能稳定到2.8V,不是3.3V,我使用的电感是10UH的,因为公司暂时没有4.7的,请问这个是不是原因所在啊
技术参数上也说电感要大于4.7UH的啊
TPS61221是输出固定3.3V的,看起来FB直接接VOUT即可,楼主能否测试下VIN,VOUT,L PIN的波形。
最好拍下波形,不过有个问题就是当你的输入电压在0.7到3.3V时,输出一直是2.8V吗?
一直是2.8V,大于3.3V后,输出跟着输入升高,两者相差0.5V左右的压差,正如第一位专家所说
谢谢各位,由于这个芯片的静态电流不满足要求,所以可能暂时不用这款芯片了,也就暂时不再研究他了,